Technical FAQs

Ask a Question

What is the catalog number of the hardware bag included with a door kit catalog number HCM48DS?<br />

The hardware bag is catalog number 80104-908-50. It contains the latch bracket for the door lock.


CTA-ID : 2047186
Was this helpful?
What can we do to improve the information ?