Technical FAQs

Ask a Question

What is the application of a double throw switch?

A double throw switch is used to provide a load with voltage from either one of two separate power sources. A typical application is a load receiving power from a Utility source that could be switched over to get power from an on-site generator source.

CTA-ID : 2047156
Was this helpful?
What can we do to improve the information ?