Technical FAQs

Ask a Question

What is the difference between a catalog number SDSA2V and an SDSA2VD Surge Arrestor?

The SDSA2V and SDSA2VD have different frequency responses. The SDSA2V is a Dual Line CATV (Cable TV) protector. The SDSA2VD is in the gigahertz band for satellite TV and is not yet available. The two are not interchangeable, and are each made for their specific application.


CTA-ID : 2047527
Was this helpful?
What can we do to improve the information ?