Technical FAQs

Ask a Question

What are the handle forces for the Powerpact R frame breaker?

Reset 256N (56 lb.)
ON 235N (53 lb.)
OFF 125N (28 lb.)


CTA-ID : 2047098
Was this helpful?
What can we do to improve the information ?