Technical FAQs

Ask a Question

What is the difference between the old MEC and MEL breakers ?

The MEC ( I-Line) or MELC were older series 100% rated breakers that became obsolete in the late 1980`s. The newer ME and MEL are all 100% rated.


CTA-ID : 2047567
Was this helpful?
What can we do to improve the information ?