Technical FAQs

Ask a Question

What is the amperage range of branch breakers that can be used in a SC816F200S?

Use 15-110A and 150-200A branch breakers only. 125A branch breakers are not allowed. Total circuit breaker handle rating not to exceed 170A per branch circuit connector.

CTA-ID : 2046966
Was this helpful?
What can we do to improve the information ?