Technical FAQs

Ask a Question

Can the base mounting rails alone be replaced on an Energy Efficient Dry Type Transformer?

Issue:
Base replacement on Transformers

Product Line:
LV Transformers

Environment:
Applies to Ventilated  Transformers by SquareD/Schneider Electric

Cause:
Transformers may have damaged mounting bases or rails

Resolution:

It depends on the enclosure used.  Smaller Energy Efficient Transformers have a base assembly and side panels that comprise the base mounting rails.  Both must be replaced if the base mounting rail area is damaged.  Larger EE Transformers have the rails as part of the base assembly, which can be replaced.  Still larger EE Transformers have individual C channel rails that may be removed and replaced.


CTA-ID : 2047757
Was this helpful?
What can we do to improve the information ?