Technical FAQs

Ask a Question

Is there a 4-20 mA output module option available for the Solid State Overloads?<br />

No. The direct mount module is obsolete. However, there is a separate current sensor called the Hawkeye from Veris Industries that can be added to the enclosed starter.

CTA-ID : 2047741
Was this helpful?
What can we do to improve the information ?