Technical FAQs

Ask a Question

Is the enclosed ATS48 available in a Non-combination style unit?

No. The enclosed ATS48 is only available in either Fusible disconnect or the circuit breaker option.


CTA-ID : 2047739
Was this helpful?
What can we do to improve the information ?