Technical FAQs

Ask a Question

Do the GV2 or GV3 manual starters have an alarm contact integral to the starter?

No. There is a fault signalling auxiliary contact available for the device but it does not distinguish between overload and short circuit. However, it will change state on either of those faults.

CTA-ID : 2046946
Was this helpful?
What can we do to improve the information ?