Technical FAQs

Ask a Question

If a HOMCGK2C, generator interlock kit, is Installed on a bottom fed main breaker Homeline load center, and the Label is oriented upside down, is there another label available that can be used, so it can be read correctly?

Issue:
Product Design Features

Product line:
Homeline load centers

Environment:
Labeling

Cause:
Customer request

Resolution:

There are No alternate labels available for the HOMCGK2C.


CTA-ID : 2046980
Was this helpful?
What can we do to improve the information ?