Technical FAQs

Ask a Question

Why are there 2 number 8`s on the micrologic series B trip unit for an LX- breaker?

On the LE there is an instantaneous off but on the LX there isn`t. They used the same switch dial for both but for the LX it doesn`t have an off feature so they put another 8 on there. Either 8 will work.


CTA-ID : 2046982
Was this helpful?
What can we do to improve the information ?