Technical FAQs

Ask a Question

Is it possible to order, other than standard, lug sizes for standard bus plugs? A bus plug such as a PBQ4660G that would accommodate 3) 3/0 conductors.

In most cases, an other than standard lug requirement can be accommodated. A request such as this is reviewed on an order by order basis. If the request is feasible, the order is processed as a special.

CTA-ID : 2047452
Was this helpful?
What can we do to improve the information ?