Technical FAQs

Ask a Question

What size lugs are on the 8903SYG17 ?

The line and load lugs accomodate 1 or 2 #4-350kcmil Cu or AL wire


CTA-ID : 2047518
Was this helpful?
What can we do to improve the information ?