Technical FAQs

Ask a Question

How do I adjust the three pole 9065 Bimetallic Overload Relays from ``Hand`` to ``Auto`` reset?

The Type S, three-element bimetallic overloads are converted from ``Hand`` to ``Auto`` by depressing the reset button and sliding the metal plate located in the insulating divider between L1 and L2 down. To convert from ``Auto`` to ``Hand``, reverse the procedure. For a picture of this see Figure 1 on page 1-139 of Digest 169, dated December, 1992.

CTA-ID : 2047655
Was this helpful?
What can we do to improve the information ?