Technical FAQs

Ask a Question

Does Motorpact wiring meet UL VW-1 vertical flame test?

Issue:
Codes/Std/Certification

Product Line:
NEMA ICS 3, UL347, EEMAC G14-1, ANSI C19.7, IEC 60470, IEC 60529, IEC60694, IEC60129, IEC62271-102, IEC 62271-200, ANSI C37.20.7 

Environment:
INMVE - MV EQUIPMENT

Cause:
Passing the UL VW-1 vertical flame test is a desirable equipment attribute.

Resolution:
Yes, the THHN wiring in Motorpact meets the UL VW-1 flame test. The wire will be imprinted with the VW-1 mark also.


CTA-ID : 2047792
Was this helpful?
What can we do to improve the information ?