Technical FAQs

Ask a Question

Does the RC816F200C contain a bypass on the meter socket?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Cause:
Meter Socket bypass type

Resolution:
A bypass is NOT provided on this device, but a horn bypass is available for field installation. Use part #MMHB if required.


CTA-ID : 2047603
Was this helpful?
What can we do to improve the information ?