Technical FAQs

Ask a Question

Can the HOM612L100S, load centers, surface cover, be used to replace the flush cover on an HOM612L100F?

Yes, you can use a surface cover on the HOM612L100F, if it is Mounted on the wall, correctly.


CTA-ID : 2047563
Was this helpful?
What can we do to improve the information ?