Technical FAQs

Ask a Question

What is the part number for the replacement module for a TVS3EMA16A?

The standard construction is as follows:
The A and C modules = MA1IMA16
The B phase module = MA3IMA16.
If the high leg is not the B phase make sure the what ever phase is the high leg in the system uses the MA3IMA16 module.

CTA-ID : 2047724
Was this helpful?
What can we do to improve the information ?