Technical FAQs

Ask a Question

Do the MG27047 and MG27048 rotary handles give a visual trip indication?

There is no ``tripped`` position but the handle will go to off when the breaker trips. There is a padlock symbol on the handle to indicate you would put it in that position to lock it in the``off`` position and there is the I symbol indicating the ``on`` position.


CTA-ID : 2047708
Was this helpful?
What can we do to improve the information ?