Technical FAQs

Ask a Question

What is the NEMA rating for the XVE Indicator Banks?

XVE line is NEMA and UL Type 12 and IP42 rated if mounted in the vertical position. XVEC21P is IP54 rated.


CTA-ID : 2047541
Was this helpful?
What can we do to improve the information ?