Technical FAQs

Ask a Question

Can you remove the horn bypass on a RC816F200CH?

Yes, the horn bypass components can be removed. However, removing the horn bypass components may possibly be considered a violation of the National Electrical Code by the local AHJ (Authority Having Jurisdiction). It would be recommended to consider using an equivalent device with no horn bypass feature, catalog number RC816F200C.


CTA-ID : 2047691
Was this helpful?
What can we do to improve the information ?