Technical FAQs

Ask a Question

Are the 9070T and 9070TF transformers CE Marked for import into the European Union?

Yes the 9070T and 9070TF transformers are CE Marked in accordance with the Low Voltage Directive.


CTA-ID : 2047408
Was this helpful?
What can we do to improve the information ?