Technical FAQs

Ask a Question

What does a H6 mean on a 9001KR1UH6?

H* codes are suffixes add to the operator partnumber so that contact blocks are installed in specific sequences to perform specific operations.
H6 means a 9001KA3 contact will be mounted in position 1 or the left side back of the push button looking from behind.

CTA-ID : 2047407
Was this helpful?
What can we do to improve the information ?