Technical FAQs

Ask a Question

What is the magnetic trip of a QO120HM and a QOB120HM?

The QO120HM and QOB120HM high magnetic breaker is calibrated so that the magnetic trip levels are between the range of 322 A to 537 A.


CTA-ID : 2047502
Was this helpful?
What can we do to improve the information ?