Technical FAQs

Ask a Question

What size wire does a catalog number NQN6CU Neutral Kit accept?

There are two lugs in the kit with wire range from 1/0-750 kcmil, Aluminum or Copper conductor.


CTA-ID : 2047498
Was this helpful?
What can we do to improve the information ?