Technical FAQs

Ask a Question

Does the CM200S include the main breaker?

No, the CM200S is not supplied with a factory installed main breaker. The main breaker must be purchased separately and field installed. Use QOM2-VH type main breaker, 200A maximum.

CTA-ID : 2047482
Was this helpful?
What can we do to improve the information ?