Technical FAQs

Ask a Question

What is the lug wire range provided on the Q Frame PowerPact circuit breakers?

Issue:
Product Features

Product Line:
Circuit Breakers

Environment:
Q Frame PowerPact Breakers

Resolution:
The lug wire range is (1) #4 AWG - 300 KCMIL aluminum or copper.


CTA-ID : 2046151
Was this helpful?
What can we do to improve the information ?