Technical FAQs

Ask a Question

Is it OK to use 15kV S&C fuses on a 4800V system?

Yes, it is OK for boric acid fuses only. For current limiting fuses, they must be at the system voltage class.

CTA-ID : 2046126
Was this helpful?
What can we do to improve the information ?