Technical FAQs

Ask a Question

Can the 5th Jaws supplied in a MPH86200 be removed on site?

If installed on a 120/240 Vac, 1-Phase, 3-Wire 600A maximum service and requested by the local utility, then yes the 5th Jaw kits may be removed from this device. NOTE: The white control wires attached to these 5th Jaw kits must also be removed. It should be noted that these 5th Jaw kits do not interfere with the operation of 4-Jaw Watt-hour Meter.


CTA-ID : 2046106
Was this helpful?
What can we do to improve the information ?