Technical FAQs

Ask a Question

Does the LC11021 have black leads or terminals?

The LC11021 has the two terminals on the left and two terminals on the right. Control wiring is provided by customer. When terminating control wires connect to one of the terminals on the left and one terminal on the right side with the voltage supply as the sets of terminals on each side are connected internally.


CTA-ID : 2046083
Was this helpful?
What can we do to improve the information ?