Technical FAQs

Ask a Question

How many fuses does the EZM1400FS require?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Fuses

Cause:
Installation

Resolution:
The EZM1400FS will accept two 300V Class T, 400A maximum, fuses (one fuse per phase).


CTA-ID : 2045557
Was this helpful?
What can we do to improve the information ?