Technical FAQs

Ask a Question

Can a pulsation plug be field installed on the 9013FGS,FHG or FYG pressure switches?

The pulsation plug can only be field installed on 9013 devices with the single 1/4`` NPSF (internal) thread pressure connection. It is not available on devices with the four way fitting, This device is not intended for use with pneumatic systems. This information is shown in our Digest 174.

CTA-ID : 2045827
Was this helpful?
What can we do to improve the information ?