Technical FAQs

Ask a Question

What is the Electrical Interlock Kit for an 82454?

An EK400DTU2 can be field installed into a 82454, Series E03. It has 2NO/2NC contacts for each ON position of the double throw switch.


CTA-ID : 2045957
Was this helpful?
What can we do to improve the information ?