Technical FAQs

Ask a Question

What is the actual length of the rolling pin style lever arm - AL1802 for the L100/L300 Limit Switches?

The roller is 3.468 inches long and the shaft is 2.625 inches long, plus there is a washer and screw that holds the rolling pin on, so the overall length would be 6.093 inches + the thickness of the washer and screw.


CTA-ID : 2045936
Was this helpful?
What can we do to improve the information ?