Technical FAQs

Ask a Question

Does the GFM100FA come with the lugs or do you have to order them separately?

The GFM100FA comes with the lugs. if replacement lugs are required order AL100FA.


CTA-ID : 2045869
Was this helpful?
What can we do to improve the information ?