Technical FAQs

Ask a Question

Can the 9421LT1 be used with the MAL/MHL361200 breaker?

Issue:
Can the 9421LT1 be used with the MAL/MHL361200 breaker?

Product Lines:
Square D Circuit Breaker, MAL, MHL, MEL, MXL

Environment:
Products sold in North America

Cause:
Determining thru the door mechanism for a MAL or MHL breaker

Resolution:
Yes, the 9421LT1 can be use on MAL and MHL breakers as well as the MEL and MXL breakers.
 
Complete Kits
Part # Handle Shaft Op. Mech
9421LT1 9421LH8 9421LS8 9421LM1
9421LT4 9421LH8 9421LS10 9421LM1

9421LT1


9421LT4


 
Handle Kit
Part # NEMA Rating Trip Indication
9421LH8 1, 3, 3R, 12 Yes
9421LH48 4 (Painted) No
9421LC48 4X (Chrome Plated) No
 
Shaft Kit
Part # Mounting Depth (in)
9421LS8 7 3/16 -11 5/8
9421LS10 7 3/16 - 22 1/4
 
Operating Mechanism
9421LM1

CTA-ID : 2045981
Was this helpful?
What can we do to improve the information ?