Technical FAQs

Ask a Question

What is the overall length of the ZCKY81 arm?

The ZCKY81 Spring Lever Arm is 3.75`` or 113.5 mm in length from the center of the mounting hole to the top of the delrin cap on the end of the spring lever.

CTA-ID : 2046293
Was this helpful?
What can we do to improve the information ?