Technical FAQs

Ask a Question

What are the repair parts for an EZM432R, Series 004, Branch Unit?

Repair parts

Product Line:

Repair parts


Only the parts listed below are considered field replaceable, and some components are no longer available:
Parts include Meter Socket through Tenant Circuit Breaker Compartment.
Quantities listed are for one position only (where part number only is given the order quantity for that part is one):

5-Jaw Meter Socket - 4052720650
Meter Socket Jaw Assembly - (4) 7329794850
Keps Nuts to secure Meter Socket Jaws - (4) 2342702001
Mounting Screws for Meter Socket - (2) 4020508201
Line Side Meter Socket Bus Connectors - 4052722350
Keps Nuts for Line Connectors - (2) 2342702001
Load Side Meter Socket Bus Connectors
SHORT Bus Connector - 4052721150
LONG BusConnector - 4052721250
Circuit Breaker Base - 4052720550
Mounting Screws for Circuit Breaker Base - (4 ) 2142717200
Branch Neutral Assembly
Lug Body - 4025110101
Wire Binding Screw 4020901401 (obsolete no longer available)
Mounting Screw for Lug - 2150718200
Bus Connector - 4052717001
Connector Keps Nut - 2342702001

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Individual Meter Socket Trim (Ring Type) - 4052793950
Gasket for Meter Socket Trim - 4052736801
Mounting Screw for Meter Socket Trim - 2142217101
Meter Socket Sealing Ring (standard aluminum snap type) - 2920910001
Circuit Breaker RB Cover (one position) - BCH (Obsolete, no longer available, no replacement)

CTA-ID : 2046234
Was this helpful?
What can we do to improve the information ?