Technical FAQs

Ask a Question

What is the p/n for the short cables for an NQOD panelboard needed to add a subfeed QBL breaker?

Issue:
What is the p/n for the short cables for an NQOD panelboard needed to add a subfeed QBL breaker?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Replacement parts.

Resolution:
On NQOD panels, if a subfeed breaker space is existing and a QBL is being added, the customer will have to supply his own cables for connecting the subfeed breaker.


CTA-ID : 2046161
Was this helpful?
What can we do to improve the information ?