Technical FAQs

Ask a Question

Do MAF, MAL, and MAP breakers have threads all the way through the terminal pads? If so, what is the thread pitch?

Yes, the ON end is tapped all the way through. For 125-400 amps, it is threaded at 3/8-16; for 450-1000 amps, it is threaded at 7/16-14.

CTA-ID : 2046036
Was this helpful?
What can we do to improve the information ?