Technical FAQs

Ask a Question

Will an HOM1RK circuit breaker retaining kit work in a smaller load center, such as an HOM24L70S?

No. The HOM1RK is not designed for installation in the smaller fixed main lug load centers. They do not use a backfed main, and have no provisions for one.


CTA-ID : 2045758
Was this helpful?
What can we do to improve the information ?