Technical FAQs

Ask a Question

Will a 225A LA circuit breaker be series rated at 22K with a 225 A MLO NQOD panel with QO-VH circuit breakers?<br /><br />

No. A 225 A LA circuit breaker will not be series rated at 22K with an NQOD MLO interior. This is a fully rated combination. Series ratings can be found on page 8-2 of Digest 173 or in the Digest Plus Selector at

CTA-ID : 2045302
Was this helpful?
What can we do to improve the information ?