Technical FAQs

Ask a Question

How do you remove a separately mounted LRD Tesys Overload Relay Block from a DIN rail?

Depending on the age of the overload relay, look for a red loop sticking out the bottom. If there is one, put a screwdriver inside the loop and pull it down.

If there is no red loop, pull down on the assembly on the rail and as you are pulling it down - rotate the bottom up toward you - freeing the bottom catch. Then lift the overload off of the DIN rail


CTA-ID : 2045136
Was this helpful?
What can we do to improve the information ?