Technical FAQs

Ask a Question

<br /><br />What is the clamping voltage on a Hard Wired Surge Arresters.

Refer to the Surge Protection Devices catalog section 6671CT9701R4/00, available on-line at www.squared.com, for technical information and product specifications.


CTA-ID : 2046037
Was this helpful?
What can we do to improve the information ?