Technical FAQs

Ask a Question

What is the overall width with Handle, of the enclosure for catalog number HU365DS Current Series?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Dimensional Information

Cause:
Installation

Resolution:
The width of the enclosure itself is 26.25" wide. The Handle of the HU365DS is located on the front flange of the switch and does NOT add to the overall width dimension.

NOTE: SEE THE CURRENT 2D CAD DRAWINGS ON-LINE FOR ALL THE DIMENSIONS.


CTA-ID : 2045767
Was this helpful?
What can we do to improve the information ?