Technical FAQs

Ask a Question

SE motor will not shut off. Replaced charging motor; same problelm.

If the springs do not charge, the motor is running because the gear on the shaft is loose. Replace the motor.
If the springs do charge, the motor is running because the cut-off switch is not functioning. The switch cannot be replaced; must replace the breaker.


CTA-ID : 2045496
Was this helpful?
What can we do to improve the information ?