Technical FAQs

Ask a Question

What is needed to connect AP413 with current AP2513G10ST

If series 3 or 4, the customer needs an I-Line to I-Line II adaptor, AF2513G12(*) *-S for Slot, B for Bolt. If Series 1, the customer will also need need two tie channels, 45218-601-01. If series 2, the customer will need two tie channels, 45218-600-01.

CTA-ID : 2045303
Was this helpful?
What can we do to improve the information ?