Technical FAQs

Ask a Question

What are the repair parts for a PAK41CTG, Series E01, ServicePak Power Outlet Panel?<br />

Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054021401
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - 4054020050 (Includes Base Assembly, Circuit Breaker(s) and Receptacles(s) below.
Base Assembly - 4054010650
Circuit Breaker - QO120GFI and QO130
Receptacle - 4054001450 (125 volt/20 amp) and 4054004450 (125 volt/30 amp)
Receptacle Mounting Screw - 2190312160 (1 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 req`d for the 125 volt/30 amp receptacle)
Neutral Bonding Screw - Not Applicable
Ground Bar - 4023017155
Ground Bar Mounting Screw - 4020594401
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 req`d)
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2045857
Was this helpful?
What can we do to improve the information ?