Technical FAQs

Ask a Question

Can a 225A main circuit breaker be installed in a QO130M200RB load center?

Issue:
Product Design Features

Product Line:
QO three phase load centers

Environment:
Main Breaker Rating

Cause:
Application

Resolution:
No. this load center has a mains rating of ONLY 200amp MAX., so a 225amp MB cannot be installed. It would violate the UL listing and void the Square D Warranty.

CTA-ID : 2045263
Was this helpful?
What can we do to improve the information ?